NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I have no problem to flash or debug the CM4 of the board. But when I'm trying to flash the CM0+ this error occurred : Error in final launch sequence:Failed to start GDB serverFailed to start GDB serverError in initializing ST-LINK device.Reason: (255...
I'm using the necleo-wb55 board.I'm trying to increase ADC measuring speed but I found that the speed for 16-bit measurement and 12-bit measurement looks the same even though 16-bit uses 256 oversampling. I checked how many measuring cycles happen us...
When you power Nucleo-WL55JC! with external 3V3 via CN6, I could see constant 120mA current consumption. Is there any way we can reduce this?
Hi all. I've got a problem when trying to flash the STM32WLE5J8I6.I am trying to run a simple blinky code and blink an onboard LED on my custom pcb.The program builds fine, connecting with the ST-Link (Nucleo-WL55JC1) and using SWD to connect to the ...
Hello, I'm trying to connect an OLED display to my STM32WL55JC by I2C but it doesn't work...I've successfully connect it with a STM32F411RE but the I2C configuration / HAL interface seams to be different between both MCU...Here my config on the STM32...
Can you use the extended advertising and scanning found in BLE 5 somehow? I have found some references to them in the code, but cannot find any defines. Do they exist? Will they be implemented?
In examples I got familiar with RF low level access is controlled by some exact coprocessor firmware. Existing coprocessor binaries provide some higher level of abstraction that seems to not include forcing signal with exact characteristics. Do I mis...
Hi, I want to use B-U585I-IOT02A as a controller for mobile robot, I use a smartphone for the remote control. For now I am using HC-05 as the bluetooth interface because I can't find out how to program the STM32WB5MMG to act similar with HC-05. Can a...