2022-04-08 6:06 AM
When you power Nucleo-WL55JC! with external 3V3 via CN6, I could see constant 120mA current consumption. Is there any way we can reduce this?
2022-04-08 6:24 AM
I have tried removing 5V_PWR jumper JP7 and no jumpers on JP4 as per the documentation but no luck
2022-04-19 8:44 AM
Hello,
Can you tell me which program you are using to reproduce your behavior please.
Have a nice day
Regards
2022-04-19 9:04 AM
LoRaWAN_End_Node application provided by ST under this path
Projects/NUCLEO-WL55JC/Applications/LoRaWAN/LoRaWAN_End_NodeThanks LAUDO and wait for your advise.
2022-05-08 7:48 PM
Is there any update on this @Louis AUDOLY as I waiting to solve of my use cases
2022-05-09 9:35 AM
Hello @digidhamu ,
Sorry for the late reply
I tested the power consumption of a nucleo board with the end_node project and my consumption were around 20mA when we did a Tx and a below 200uA when nothing happen.
Don't you have any expansion board connected to the nucleo ?
Best regards
2022-05-12 6:52 PM
Thanks @Louis AUDOLY I didn't connect any expansion board. Would it possible to send picture of your setup and this will help me to report you back faster?