STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

Setup for LoraWan Class B support

Does STM have a recommended test setup for LoraWan Class B support testing/development? I understand that the STM32WL should support Class B, but it is very difficult to find much documentation on *Gateways* that currently support Class B (beaconing,...

JRhee.1 by Associate
  • 1740 Views
  • 2 replies
  • 0 kudos

Is there a way to broadcast message in ZigBee network using STM32WB or somehow get end devises list?

I have a network consisting of a Amazon Alexa coordinator and couple of end devices. And I need to communicate somehow between end devices directly, without coordinator. So I am trying to use APS functionality. But when I try to use the broadcast add...

ZigBee callback not working

Hi,I am using a STM32WB55 board and its USB Dongle.I set up a ZigBee network with Messaging Cluster between them.The WB55 is the router + server, and the Dongle is the coordinator + client.I can send a Message from WB to Dongle.When I try to send dat...

CDeve.2 by Associate II
  • 1149 Views
  • 1 replies
  • 0 kudos

STM32 WLE5 VBat measurement at low temperatures

Hi,I am currently doing some tests measuring the battery voltage on a system using the STM32WLE5, I am measuring both v_sys and v_bat. I am running into an issue with the v_bat measurement, I am seeing alot of noise compared to the v_sys measurement....

0693W00000NpF3iQAF.png 0693W00000NpF1SQAV.png
HWickham by Associate II
  • 1476 Views
  • 1 replies
  • 0 kudos

BLE PairingTime

Hello, I have a BLE Secure Connection implemented between an android phone and STM32WB55. Currently, using fixed key to start pairing, it takes approximately 2 seconds to get paired (after the key is sent, and devices are paired) in addition to 600ms...

Amogh by Associate III
  • 1906 Views
  • 2 replies
  • 0 kudos

STM32WLE5CC goes into unknown state

We have developed battery operated product using STM32WLE5CC.when device goes into deep sleep around 1.7uA current are flow normally.During Testing of product we face an issue which is described as below.During deep sleep of STM32WLE5CC, we removed b...

DBhut.1 by Senior
  • 1189 Views
  • 2 replies
  • 0 kudos

TIMx_RCR IRQ?

I am using TIM16 as a one second counter on an STM32WB55. I would like to generate an interrupt after it rolls x times (as example 2). I set the TIMx_RCR to a 1. Can someone tell me what function I need to call in the HAL library and should I plac...

SWenn.1 by Senior III
  • 810 Views
  • 2 replies
  • 0 kudos