2022-05-12 12:41 AM
2022-05-12 5:54 AM
OK, now at least some parameters are given so that you can achieve ranges between 10...20km, when used with an appropriate antenna. Depending on the environmental conditions, other ranges are also possible. Also, you must not forget that the data rate plays a major role: for the 10...20km mentioned with LoRa, that is about 200bit/s.
2022-05-12 5:38 AM
Welcome, @AYous.3, to the community!
Of course, you cannot find any information on this in the data sheet. Even if the range is specified for a finished module, i.e. a complete radio system including antenna, this always applies under certain conditions. The range of a radio system and thus also of a system based on STM32WLE depends on many factors:
Does it answer your question?
It might be helpful to know what you actually want to achieve so that someone can help you.
Regards
/Peter
2022-05-12 5:44 AM
@Peter BENSCH Thanks for your help,
I'm not looking for a specified information because I know that It depends on many parameters. But I wanted to know approximately the range of this transceiver, in an open area for example with a 14 dBm as an output power using LoRa.
2022-05-12 5:44 AM
Depends on a lot of factors.
15 km LoS should be demonstrable, perhaps 30 km LoS with effort and suitable conditions/terrain. Vertically perhaps to the edge of space.
2022-05-12 5:46 AM
@Community member Thanks a lot
2022-05-12 5:54 AM
OK, now at least some parameters are given so that you can achieve ranges between 10...20km, when used with an appropriate antenna. Depending on the environmental conditions, other ranges are also possible. Also, you must not forget that the data rate plays a major role: for the 10...20km mentioned with LoRa, that is about 200bit/s.
2022-05-12 6:08 AM
@Peter BENSCH Great ... Thanks a lot.
2022-05-12 6:21 AM
It looks like your question has been answered?
If the problem is resolved, please mark this topic as answered by selecting Select as best under your preferred answer(s). This will help other users find that answer faster.
Good luck!
/Peter