STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 221 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4067 Views
  • 0 replies
  • 3 kudos

Resolved! BLE sending more data than expected

Hello, I am trying to achieve high throughput on a custom board. I partially replicated BLE_Throughput example for an initial testing.I am receiving the BLE data in MATLAB. In CubeMX, I use a custom ble template. I am trying send a payload 1000x time...

Resolved! Zephyr support for STM32WB09

Are there any plans to add Zephyr support for the STM32WB0X line of chips? Or is it already supported with the current HAL? I couldn't find any Zephyr related information on the product page.

AYM1607 by Associate
  • 1744 Views
  • 1 replies
  • 1 kudos

Resolved! NOD_WL55JC LoRaWAN FUOTA fragments error

Hi,we are working on NOD_WL55JC for LoRaWAN network with FUOTA.we are facing problem when at the following condition1) development kit used NOD_WL55JC, firmware ( en.stm32cubewl-v1-3-0.zip) - en.stm32cubewl-v1-3-0\STM32Cube_FW_WL_V1.3.0\Projects\NUCL...

Couldn't Find Mac_802_15_4_Sniffer.bin file

Hi Community,I’m trying to use the CubeMonitor-RF sniffing tool to monitor packets between my two NUCLEO-WB55 boards. I have followed all the instructions indicated by UM2288 and the ST Wiki. However, I am confused about the firmware upgrade for the ...

iFoX by Associate II
  • 2124 Views
  • 3 replies
  • 0 kudos

Disabling TCXO in the software

I am using the B-L072Z-LRWAN1 and trying to optimize for low power consumption. So far I have set up the hardware by desolding SB37, SB18, R26, and D2. Now when moving JP9 from pos. 2-3 to pos. 1-2 (i.e. TCXO powered from PA12 instead of VDD_RF_LRA),...