User Activity

Hello,Configuring the I2S on CubeMX on STM32G431, for which I've connected a microphone in PDM, I want a sampling frequency of 48KHz@16bit.Typically, this requires a PDM frequency of 3.072MHz and a decimation of 64.I wonder why I need to tell CubeMX ...
Hi, I'm working on an OTA BLE bootloader for the STM32WB5MM module.I created from scratch with STM32CubeMX the same code as the OTA example for NUCLEO-WB55.I'm on BLE stack 1.21So far so good, I can update with the smartphone app.The problem I'm havi...
Hello, I'm trying to do a quick test with the STM32F412G-Discovery kit and the analogue microphone input.I use this example https://github.com/STMicroelectronics/STM32CubeF4/tree/master/Projects/STM32F412G-Discovery/Examples/BSPwith the menu #### AUD...
Hello, I'm testing the STM3240G-eval with the USB host MTP. The goal is to retrieve the photo from a canon EOS 100.The camera uses PTP protocol.As the demonstration  code read .wav file, I wrote a wav file to the root of the SD card. The digital came...
Hello,In a Client(Router)/Server configuration with two STM32WB55 I would like to accelerate the transmission of data at starting of the server.The server address is know in advance and stored in the client then in the HCI_LE_ADVERTISING_REPORT_SUBEV...
Kudos from
Kudos given to