User Activity

@ST Community @STTwo-32 @Tinnagit @Tesla DeLorean 1) I have done few changes from "#define LORAWAN_DEFAULT_CLASS CLASS_A" to "#define LORAWAN_DEFAULT_CLASS CLASS_C" in the "lora_app.h" file and I also changed "#define DISABLE_LORAWAN_RX_WINDOW 0" to ...
1) Class A for Unicast.Class B synchronous transmission (thanks to beacon) for Unicast or Multicast.Class C for continuous transmission for Unicast or Multicast.According to this details will Class C will give little bit more data rate then Class B?2...
Hello @STTwo-32  @ST Community Looking for information and details on this.1) Currently I'm using B-L072Z LRWAN1 and I'm looking forward to using WL55JC1, using WL55JC1 CLASS B will increase my data rate?2) Does WL55JC1 support CLASS B and as well as...
Hello @ST Community @STM Community Currently, I'm using Lorawan gateway: P-nucleo LRAWAN1 and Lorawan node: B-L072Z LRWAN1. As Lorawan provides a maximum range of 10 Km and a data rate of 5kbps at 125 kHz.B-L072Z node as a buffer of size 242 bytes.I ...
Hello community,Currently, I have Lorawan gateway: p-nucleo-LRWAN1 and Lorawan node: B-L072Z LRWAN1.I'm looking forward to suggestions from you, which company gateway and node will be better than this current gateway and node. with current devices, I...
Kudos from