MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem with Unicleo GUI

Hello . I have to boards L476RG and 303RE and of course IKS01A3 . After installing Unicleo , I can't connect to that IKS (It's not even showing port )  . I'm changing boards but still It can't see it . On some tutorials some lady was coping some file...

Reading LIS2DE12 temperature always reads 0

Hi all,I'm currently not able to read the temperature of my lis2de12.It always returns zero. lis2de12_temperature_meas_set(&dev_ctx, LIS2DE12_TEMP_ENABLE);lis2de12_data_rate_set(&dev_ctx, LIS2DE12_ODR_400Hz );lis2de12_block_data_update_set(&dev_ctx, ...

TEK00003.PNG
WSpar.1 by Associate III
  • 948 Views
  • 3 replies
  • 0 kudos

Resolved! LSM6DSOXTR Thermal Resistance

Hi Please can you advise on the Thermal Resistance (K/W) of LSM6DSOXTR please so we can complete our ATEx evaluation. Many Thanks Dominic

Resolved! LIS2DH12 Acceleration values

Hello,LIS2DH12 accelerometer. AN5005 datasheet. How is the data in the table in column 1 (Acceleration values) calculated? (See Figure 1). I read the calculation process in the datasheet above, but did not understand it. (See Figure 2).

Resolved! IMP34DT05 returns only silence

Hi, I am reading from IMP34DT05 (master receive, PDM), and I always receive 0x00 0x7F 0xFF 0xFF ...and 0xFF's, ever after, until reset of SAI (disable-enable). Playing sound into mic has no effect. In debugger, immediately upon SAI enabled, FIFO is f...

deno1_0-1708522103520.png deno1_1-1708522425239.png
deno1 by Associate
  • 1628 Views
  • 2 replies
  • 0 kudos

LIS3MDL magnetometer output becomes noisy after a bit

Dear community,I am trying to detect metalic objects (train axles) that are passing above two LIS3MDL sensors. For this purpose I am using LIS3MDL breakout boards from PololuWhat I notice is that often, what seems randomly, the signal becomes noisy d...

Screenshot 2024-02-08 130041.png
dburgt98 by Associate II
  • 1460 Views
  • 3 replies
  • 0 kudos

Resolved! sths34pf80 + lens

Hi!We are working on product that needs to count people on the range of 3-4 meters. We designed dev.board for sths34pf80 and tetsted it with UNICO-GUI. The max range that we are getting is around two meters and therefore it looks that we need to use ...

apallo_0-1693465987293.png
apallo by Associate
  • 2576 Views
  • 5 replies
  • 0 kudos

lsm6dso Tap detection

I tried running the code present in the github link -  https://github.com/STMicroelectronics/STMems_Standard_C_drivers/blob/master/lsm6dso_STdC/examples/lsm6dso_tap.cfor Tap detection. But in the logs, I'm not able to see the axis/sign, even after ta...

Varsha by Associate III
  • 1677 Views
  • 5 replies
  • 1 kudos

Resolved! lsm6dsox embedded features

Is it possible to execute features such as pedometer, activity/inactivity detection, tilt/tap, with same configuration of ODR, Full scale? How can I include all these features in a single program?Can someone explain this please

Varsha by Associate III
  • 1123 Views
  • 3 replies
  • 1 kudos