MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

AIS2IH VDD_IO Supply Current

Hello,What is the supply current into the VDD_IO pin on the AIS2IH? The VDD supply current requirements are explained in detail, but I do not see any note on the current into the VDD_IO pin.Best regards

Resolved! St-mems-android-linux-sensors-hal Snapdragon ADSP compatibility

Hi,From the following repo https://github.com/STMicroelectronics/st-mems-android-linux-sensors-hal/tree/masterI would like to know if the driver it's compatible with an Android environment under snapdragon where all the sensors part is managed under ...

DevM by Associate II
  • 1609 Views
  • 2 replies
  • 0 kudos

[iis3dwb] Read sensor data without loss.

Hi, I want to receive data coming from the sensor without loss.For the testing, sampling rate is set to 32Hz.26667(ODR) / 800 = 32hzif set like this, 32 data per second will be accumulated in the buffer.and CNT_BDR_THR was set to 100.also, FIFO_MODE ...

HKim23_0-1710154197476.png
HKim.23 by Associate III
  • 1497 Views
  • 4 replies
  • 1 kudos

Resolved! [IIS3DWB] Sampling rate set to 2K band.

Hi,I want to set the raw data to around 2k bandwidth and receive all data through FIFO.From what I understand, to set it to 2k bandwidth-Bandwidth ODR/4 = 2.6kHz, HPCF_XL = 0, LPF2_XL_EN =1-FIFO_CTRL3 BDR_XL = 0b1010 ( 26667Hz ) And at this time, if ...

HKim.23 by Associate III
  • 955 Views
  • 2 replies
  • 0 kudos