Skip to main content
Associate
March 12, 2024
Question

IIS3DWB offset calibration is missing

  • March 12, 2024
  • 2 replies
  • 832 views

Hello All,

is it normal that the data in the offset calibration registers disappears after a power restart?

 

 

This topic has been closed for replies.

2 replies

Federica Bossi
ST Technical Moderator
March 12, 2024

Hi @Pavel_Levkoev ,

Welcome to ST Community!

Do you mean registers: 73h, 74h, 75h?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Associate
March 12, 2024

Yes exactly,  and register  CTRL6_C (15h) with USR_OFF_W bit.

at the moment, I have to save calibration values to non-volatile memory and set them every initialization. It seems to me that something is wrong here, because logically such calibration is mainly used for correction and displacement after soldering/assembly. I.e. ideally only once.