Hello,What is the supply current into the VDD_IO pin on the AIS2IH? The VDD supply current requirements are explained in detail, but I do not see any note on the current into the VDD_IO pin.Best regards
Hello,Can you provide FIT rate data and pin FMEA for the M24C04-A125 EEPROM devices? M24C04-DRMN3TP/KM24C04-DRDW3TP/KM24C04-DRMF3TG/KThank you and best regards,Jessica Riley
Just following up on this: can you please confirm that the VDDIO current is higher in low power mode than in high performance mode (570mA vs. 28mA)? Or is the current in low power mode actually 570uA?Thanks!
Hello Federica,If you could give me typical and maximum values for 1) high performance mode and 2) low power mode w/ ODR=1.6Hz that would be very helpful. VDD=VDDIO=3.3V for both.Thank you!Jessica