MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

asm330lhh gyroscope

hello Good Morning,       i'm working on asm330lhh imu sensor, i want to get output in angle from raw value. please give suggetion and if you source code of imu sensor so share here.  

LIS2DH12 acceleration data not changing

Dear All, I am using the LIS2DH12 accelerometer that is incorporated within a Decawave DWM1001-DEV board. I am attempting to write a C program using the dwm.h library functions to display the acceleration values for the X, Y and Z axes via I2C consta...

GChan_02_0-1711436593131.png GChan_02_1-1711437056735.png GChan_02_2-1711437118612.png
GChan_02 by Associate
  • 1119 Views
  • 1 replies
  • 0 kudos

Query regarding IMU sensor for Golf Swing Analyses

Posted on October 23, 2015 at 08:33I am in search of 6 or 9 axis IMU mems sensor for golf swing analyses device. The device would be somewhat like  http://3bayslife.com/zone-1/ Should I go for 6 axis DOF or 9 axis DOF? Low power operation is must. A...

rahul23 by Associate
  • 1060 Views
  • 3 replies
  • 0 kudos

MotionVC Lib Implementation & Data Drifting

Hi all, I am trying to use the MotionVC library functions to return my vertical speed and calibrated speed, however I have encountered two unknowns: the internal timing or buffer processing of the MotionVC_Update() function and why the calibrated alt...

LIS3DH using I2C HAL - Not reading acceleration data

Hi everyone,Based on the drivers from ST GitHub, I developed my own one, but I can't understand why it's not working. I can communicate with the accelerometer and I can read the registers, but I don't know why i am having troubles to read the acceler...

LaraCS by Associate II
  • 1346 Views
  • 4 replies
  • 1 kudos

ASM330LHHX stops transmitting after some time.

I am using Nucleo F767ZI with SPI interface to ASM330LHHX sensor. I am using example code from https://github.com/STMicroelectronics/STMems_Standard_C_drivers/blob/master/asm330lhhx_STdC/examples/asm330lhhx_read_data_polling.cAfter a couple of second...

MAnto.2 by Associate III
  • 960 Views
  • 2 replies
  • 2 kudos

Resolved! L3gd20 sensor on stm32f411e-discovery

I am practicing reading L3GD20 data built into the stm32f411e-discovery kit. I use SPI1 to communicate with L3GD20. I watched on YouTube, they have instructions on how to use the void function HAL_GPIO_EXTI_Callback. I cannot call the void HAL_GPIO_E...

image.png image.png image.png image.png