MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LSM6DSO32X and INT1

If I am trying to use INT1 to indicate a "data-ready" event, does that result in a Low to High transition on the INT1 pin? Or a High to Low transition on the INT1 pin?  Does the line stay high indefinitely, until the data is read? What happens when n...

Dude by Associate III
  • 713 Views
  • 1 replies
  • 0 kudos

LIS3DH Tilt and upside down detection

Hi all,I'm trying to use the LIS3DH to detect if the object is in a non-safe position, i.e. standing on a slope (tilted) or in the upside down position and generates an interrupt if it's one of these. Setup:Y-axis pointing downwards in the stable pos...

Vibration speed and acceleration in time domain

There are two parameters "Speed" and "Acceleration Peak" in time domain (using MotionSP library). What condition (e.g. frequency 10Hz - 1kHz use speed and Above 1kHz use acceleration peak) will be used Speed in time domain and Acc Peak in time domai...

0693W00000ANx4hQAD.png
JTam.1 by Associate II
  • 924 Views
  • 2 replies
  • 0 kudos

ASM330LHH gyroscope always sent 0 after few second

Hi I use a nucleo L432KC for a POC with an ASM330LHH. I use the internal FIFO of the ASM330 to store accelerator and gyroscope datas. I use an SPI to get datas periodically.During developpment, we used the 3.3V of the nucleo to supply the ASM330. We ...

dlb_0-1711094766109.png dlb_1-1711094795018.png
dlb by Associate II
  • 1221 Views
  • 3 replies
  • 0 kudos

Resolved! ST LIS3DH schematic review

Hello ST Community, I am currently working on a flight computer for a model rocket. It will be used together with a barometric pressure to estimate the altitude. It would be very nice if someone could review my schematic and point out any mistakes.  ...

Fazeli24_0-1711042284745.png
Fazeli24 by Associate
  • 1159 Views
  • 2 replies
  • 0 kudos

Resolved! lsm6dso 6d/4d orientation

Is it necessary to enable Free Fall detection in order to detect orientation changes? What role does Free Fall (FF) play in this context? Additionally, is there a way to set a threshold force for detecting orientation changes, such as when the IMU is...

Varsha by Associate III
  • 1627 Views
  • 5 replies
  • 1 kudos

LIS2DW12 using iio buffer, + temperature channel

Hi Problems with a iio interface and using of buffer. Goal use the iio buffer interface for accel x y, z and temperture values.    Include one Channel more for the temperature.     static const struct iio_chan_spec st_accel_12bit_channels_temp[] = {S...

KScha.3 by Associate II
  • 895 Views
  • 3 replies
  • 0 kudos

[iis3dwb] What are the units of the BDR_XL registor?

Adjusting the register values below seems to adjust the time at which data is written to the buffer. I understood that the value is similar to Data Sampling frequency.If i set the value to 6, about 1900 data per second will be written to the buffer.I...

HKim23_0-1710207022327.png
HKim.23 by Associate III
  • 999 Views
  • 3 replies
  • 0 kudos