cancel
Showing results for 
Search instead for 
Did you mean: 

Query regarding IMU sensor for Golf Swing Analyses

rahul23
Associate
Posted on October 23, 2015 at 08:33

I am in search of 6 or 9 axis IMU mems sensor for golf swing analyses device.

The device would be somewhat like  http://3bayslife.com/zone-1/ 

Should I go for 6 axis DOF or 9 axis DOF? Low power operation is must. 

Also the captured data is to be transmitted via bluetooth to smartphone. 

Suggest me with suitable options for 6 or 9 axis MEMs (which one is better and why?) and also the bluetooth socs that are suitable for this project.

#golf-swing-analyses
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
rahul23
Associate
Posted on October 29, 2015 at 08:56

Unfortunately, I do not see any replies coming. 

This is my first post on ST community. 

oyvind2
Associate II
Posted on October 29, 2015 at 09:53

Unfortunately, this forum is not very useful. Perhaps you should try invensense or bosch.

Elben
Associate

I also need a device to analyze the golf swing so I can video it and put it on YouTube. Where can I get this device?