User Activity

I want to test X-Nucleo IKS02A1 board with MEMS Studio. I tried to connect to 4 different boards:-Nucleo F767ZI,-Nucleo F446RE,-Nucleo L053R8 ,-Nucleo WB15CC,I always get the same error:Some device is already connectedWhat can I  do. Is this some lin...
I am using Nucleo F767ZI with SPI interface to ASM330LHHX sensor. I am using example code from https://github.com/STMicroelectronics/STMems_Standard_C_drivers/blob/master/asm330lhhx_STdC/examples/asm330lhhx_read_data_polling.cAfter a couple of second...
I converted project from C to C++ with right click on project-> Convert to C++. The problem occurs when I generate the code in graphic configurator . It creates main.c file. Which is also loaded to controller if I run it. How to solve this problem?
Because of nature of my application sometimes I need to disconnect the cable for UART. In tthat case frame error is detected (sometimes noise or overrun). I would like that after reconnection of the cable UART communication comes back. After reconnec...
Kudos from
Kudos given to