MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to increase ODR and Buffer Size of ISM330IS

As mentioned in the datasheet of ISM330IS, we can go to accelerometer ODR of 6667 Hz but in the NanoEdge AI Studio, it is showing only upto 833 Hz. Can you tell how can we go above ODR of 833 and the. Also how can we go above Sample per axis i.e. buf...

jayantver_0-1716554823974.png jayantver_1-1716554823963.png

MotionFx ATime, MTime and FrTime Parameter

I'm currently trying to stabilize the MotionFx Sensorfusion in an environment with medium magnetic disturbances. However I don't quite understand the three parameters ATime, MTime and FrTime from the Knobs structure. For example the manual UM2220 des...

ritzmo93 by Associate
  • 612 Views
  • 0 replies
  • 0 kudos

LSM6DS3 SPI communication problem with STM32F4

Привіт! У мене проблема з отриманням даних із датчика LSM6DS3. Коли я намагаюся прочитати значення реєстру "WHO_AM_I", я отримую надто короткі імпульси у відповідь, які не можуть бути прочитані поданими до його тактового сигналу.Я використовую цю пла...

DmytroMachkovskyi_0-1716675423212.png DmytroMachkovskyi_1-1716676173880.png DmytroMachkovskyi_2-1716676417924.png DmytroMachkovskyi_3-1716676549564.png

Resolved! Unicleo-GUI datalog's timestamp not working correctly

I'm working with a nucleo 401RE and a x-nucleo ISK 01A3 as hardware and algobuilder and unicleo-GUI as software. If I measure, for example, the rotation vector 9X throughout the day and save the output datalog using Unicleo-GUI, the timestamp shows t...

aesteban by Associate III
  • 791 Views
  • 1 replies
  • 0 kudos

Resolved! Issue while configuring the example of lis2dw12 sensor

HiI am trying to configure the accelerometer sensor to read the data polling  as the example suggested in githubWhen I try to read /* Read output only if new value is available */lis2dw12_flag_data_ready_get(&dev_ctx, &reg);At initial the drdy will b...

M4n0j by Associate
  • 1115 Views
  • 2 replies
  • 0 kudos

Resolved! Getting started with STEVAL-MIC007V1

Hi Everybody, I am a beginner and I need some information to start using the following devices:- Nucleo-F401RE- X-Nucleo-Amicam1- Steval-mic007v1. I have currently downloaded the following material:- X-cube-memsmic1- Link007- Link009- Stm32cubeid.Is ...

OsBo by Associate
  • 791 Views
  • 1 replies
  • 0 kudos