MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS2DTW12 temperature sensor accuracy

Hello everyone,We manufactured about 100 boards for a pre-production run using the LIS2DTW12, and at room temperature, the boards are all over the map with +/-3°C accuracy, nowhere near the "typical" +/-0.8°C as stated in the datasheet.I've already s...

vard by Associate II
  • 2613 Views
  • 6 replies
  • 1 kudos

Resolved! Signal delay MEMS Studio BUG

I think signal delay library does not work on MEMS Studio.I made an example code to show temperature values from a nucleo-L476RG and x-nucleo-IKS01A3 setup.The code should show the actual value and a delayed one:But it gives the following error:This ...

aesteban_0-1715168691138.png aesteban_1-1715168772554.png
aesteban by Associate III
  • 769 Views
  • 1 replies
  • 0 kudos

IMU long term stability

Hi,I encountered a problem with a couple of LSM6DSOX employed over 2 years in a mobile Hydraulcs application where the came back to factory for inspection and we saw a significant drift of the offset of the accelerometer (>200mg).Looking at the ASM33...

gioPic97 by Associate
  • 1028 Views
  • 1 replies
  • 0 kudos

Resolved! LIS2DW12's sensitivity setting

Hi,I am using LIS2DW12 to detect walking situation of old man.Old man is walking slowly and little moving, In order to detect this small moving, what and how do I set CTRL register you recommend?I have to check continuous moving state....If LIS2DW12 ...

Paul.Lee by Associate III
  • 2111 Views
  • 7 replies
  • 0 kudos

vibration monitoring with ASM330LHH

hello,  i'm working on asm330lhh imu sensor and s32k324 nxp microcontroller.Microcontroller : s32k324imu sensor : ASM330LHHinterface : SPI     Question  1. i want to monitor vibration with this imu sensor. how can i implement code give me vibration m...