MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

sensortile.box PRO connectiong via bluetooth

Hello everyone! It's my first time with the Sensortile.box, and I'm still not clear on how to connect via Bluetooth. Inside my Sensortile.box, I have the firmware STSW-MKBOXPRO V1.1.0, and from the ST BLE Sensor application, I'm able to see the box. ...

Frabbit by Associate III
  • 1420 Views
  • 4 replies
  • 1 kudos

Resolved! App Crashes when Uploading App from Expert Mode

Hi all, I have been playing around with a SensorTile.Box PRO and have had success in uploading the premade "apps" provided in the app itself. However, when I create a custom app in Expert mode and try to upload it to the unit, the app crashes and the...

ZoeTakacs by Associate II
  • 1860 Views
  • 5 replies
  • 1 kudos

Resolved! I want to control same sensor in same I2C Bus.

 I use STM32F401RE nucleo board to detect tilt. I will use same MEMS sensor (ISM330DLC). Three. But I want to control that sensor in I2C1 Bus.  I know setting SA0 to distinguish SAD. it's only possible to two devices.  I need to control three devices...

sonja by Associate II
  • 800 Views
  • 1 replies
  • 0 kudos

STEVAL- MKBOXPRO

Hi team,Can we connect the STEVAL- MKE001A add on board with STEVAL- MKBOXPRO(It has DIL24 sensor adapter socket) to collect the fusion data from LSM6DSO16IS IMU?

head tracking

Hi team Is there development board available for Head tracking feature?  I have sensor tile box pro also I am able to get fusion output from that, can I get head tracking output from that?

lis2HH12 movement detect

Hi All,I have a prototype pcb with lis2hh12 + stm32 and i want to configure movement detection into the accell but all informations that i found was about ACT_THS (1Eh) and ACT_DUR (1Fh).In my tests accel does not set INT1 (as desired)... Do anyone k...

WBria.1 by Associate II
  • 827 Views
  • 1 replies
  • 0 kudos

LIS2DW12 celestial gravity

HelloIf a device using LIS2DW12 is fixed in a fixed position, will it be affected by the gravitational pull of the sun or moon and will the gravitational acceleration of each axis change?

meco by Associate II
  • 844 Views
  • 2 replies
  • 0 kudos