MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Accelerometer and gyroscope reading using sensor

Hi,I want to know the best solution to read accelerometer and gyroscope data using the STEVAL-MKI182V2 board with the STEVAL-MKI109V3. At this moment, I can use Unico-GUI to read live all the data from the sensor, but I want to make a AI model to rea...

unable to connect STEVAL MKBOXPROA to mems studio

Hi,I'm unable to connect my STEVAL MKBOXPROA  (SensorTile.Box Pro) to Mems Studio, here's what I get:"board not identified" I tried uploading the DataLogExtended.bin, and it says it programs successfully, but I noticed there's a quick "verification f...

Keef_0-1718150019155.png Keef_2-1718150133684.png
Keef by Associate II
  • 1137 Views
  • 3 replies
  • 0 kudos

How to use Unicleo-GUI with X-NUCLEO-IKS02A1?

My customer asked me to assess some ST MEMS products using a project he found on Github: https://github.com/STMicroelectronics/X-CUBE-MEMS1/tree/main/Projects/NUCLEO-L152RE/Applications/IKS01A3/FitnessActivitiesThis advised to purchase a Nucleo L152R...

LSM6DSOX - getting quaternions

LSM6DSOX is a really powerful chip for detecting events, but i also wanted to get quaternions out of it without having to do any math on raw IMU data.   So this is what i found Example IMU driver  Register 59H - TAP_THS-6D,  You can enabled 4D/6D pos...

BA_ by Associate II
  • 741 Views
  • 0 replies
  • 0 kudos

Resolved! SensorTile.box does not power up after FOTA firmware upload

I have a big issue with the STEVAL MKSBOX1V1. I was making some attempts to work with the Vibration Monitoring Example (made up of "Training" and "Compare" sub-processes). After having successfully run the example on the firmware preloaded on the Sen...

francus76 by Associate III
  • 2093 Views
  • 6 replies
  • 1 kudos

Resolved! MEMS studio & STEVAL-STWIN KT1B

does MEMS studio support STEVAL-STWIN KT1B board ; cause according to the UM (https://www.st.com/resource/en/user_manual/um3233-getting-started-with-memsstudio-stmicroelectronics.pdf) only STEVAL-STWIN KT1 Hardware compatible (not with full/reduced s...

Resolved! Question for LPS25HB Pin#7 connection

I am designing to mount LPS25HB on the board.Communication is I2C.Please help me with the connection of Pin 7 (INT_DRDY).Is this pin an open pad? Or does it need to be connected to GND?

genki by Associate
  • 772 Views
  • 1 replies
  • 1 kudos

LIS2DW12TR overheating when connected with I2C

I have 4 LIS2DW12TR accelerometers connected to an Seeed Studio ESP-32 S3. The accelerometers get extremely hot when they're connected to 3.3V. They are not recognised with an I2C scan.The accelerometers are connected to 2 pairs of SDA/SCL pins. Each...

Screenshot 2024-06-07 at 9.32.39 PM.png Screenshot 2024-06-07 at 9.32.39 PM.png Screenshot 2024-06-07 at 9.37.16 PM.png Screenshot 2024-06-07 at 9.37.22 PM.png