User Activity

Hello,section "4.5.1 Example of output data" of the LIS2DUX12 device application note (AN5909) provides an example of calculating the acceleration value from the FIFO.In the example 14 useful bytes from the FIFO are multiplied by the sensitivity in "...
Hello,the LIS2DUX12 documentation (AN5903: LIS2DUX12: machine learning core) contains a table explaining how meta-classifier works:At the third column from the end of the table, the decision tree gives the result "A".As far as I understand, the "B" c...
Hello,The LIS2DUX12 datasheet clearly states that "12.1.3 FSM_START_ADD_L (58h) and FSM_START_ADD_H (59h) FSM start address register (R/W). First available address is 0x35C.".The default address in MEMS-studio is 0x0200. In the FSM examples on GitHub...
Hello,I want to enter the decimal part of a number in to filed "Float" (Advanced Features -> FSM -> Converter).The Decimal Separator in the Regional Settings of the system I use (KDE/plasma) is a comma.It seems that the "Float" field only accepts a d...
Hello,in KDE/plasma environment I can't use MEMS-studio because it doesn't show file dialogs.For example: MEMS-studio is connected to the STEVAL-MKI109V3 board, in "Advanced Features" -> "FSM" I click the "Load state machine from file“ button, but no...
Kudos from
Kudos given to