MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

4D/6D threshold setting for LIS2DS12

Posted on July 07, 2017 at 02:25Dear sir/madam,I'm confused how the Threshold decodeing(degrees) comes like shown in LIS2DS12 datasheet, page 31. When 6 stands for 80 degrees and how 6 comes from?I try to use 60 degrees threshold and I can read accu...

0690X00000603kIQAQ.jpg

LIS3MDL_Interrupt problem

Posted on September 03, 2017 at 10:27Hello sir,HELLO EVERYBODY,I have a question about LIS3MDL.   Expecially, interrupt problem.I am using LIS3MDL below sequence.=================================================================================1. In ...

LIS2DH FIFO in SPI mode

Posted on July 13, 2017 at 14:06I did not quite understand from the pdf when reading 32*3 samples from the FIFO in SPI mode, can I set the SPI starting address at OUT_X_L (28h) with the SPI's MS bit raised and then read in a constant SPI read stream...

I am using LIS3MDL and is there any way to offset the interrupt threshold values by changing the Offset Registers? What I mean is suppose my surrounding environment z-axis value is 50uT and if I want to offset it to 0 then I can write 50uT to the OFFSET

Posted on July 22, 2017 at 08:34I am using LIS3MDL and is there any way to offset the interrupt threshold values by changing the Offset Registers? What I mean is suppose my surrounding environment z-axis value is 50uT and if I want to offset it to 0...

Reading data from LSM303AGR

Posted on June 22, 2017 at 15:50Hi, I'm new here and I am new at working on mems.I have a LPCXpresso1549 evaluation board and a Steval-MKI172v1 mems that implements a lsm303agr chip. I'm working on mbed platform and I need to read values from accele...

LSM9DS1 I2C address identification

Posted on June 22, 2017 at 09:56Hi,I am planning to use  LSM9DS1 9DoF sensor in our project. As per datasheet table #2, Least significant bit for I2C address is [SDO_   A/G or SDO_M ]= SA0.From this information & Table#19, I will be able to identify...

LSM6DS3US bootup delay

Posted on July 27, 2017 at 07:27Hi,I am 'LSM6DS3US' sensor only for Gyroscope in I2C mode.I have the following queries related to the Gyro:1. After Power On is �20ms� delay needed for bootup procedure to load trimming parameters.Is this delay mandat...

I am curious about the power consumption of the LSM6DS3.

Posted on August 21, 2017 at 16:33Hello.I am curious about the power consumption of the LSM6DS3. The LSM6DS3 can set ODR independently.However, the power consumption when the ODR is set independently is not listed in the Application note.Only <Accel...

Is the LSM6DS3 accurate enough for human body motion tracking?

Posted on September 01, 2017 at 10:37My previous MEMs system is based on LSM6DS3(+-2000dps scale). According to my experimental data, if I rotated the sensor slowly by hands, the integrated attitude of gyroscope data was quite accurate and acceptabl...

VL53L0X: Possible to change I2C address permanently?

Posted on August 29, 2017 at 18:30Hi everybody!Just a short question about the VL53L0X Time-of-Flight ranging and gesture detection sensor.The datasheet mentions a 'Programmable I2C address'.Is it possible to change the default I2C address to anothe...

Tob G by Associate II
  • 3145 Views
  • 3 replies
  • 0 kudos