cancel
Showing results for 
Search instead for 
Did you mean: 

I am curious about the power consumption of the LSM6DS3.

Seung-jin Lee
Associate
Posted on August 21, 2017 at 16:33

Hello.

I am curious about the power consumption of the LSM6DS3. 

The LSM6DS3 can set ODR independently.

However, the power consumption when the ODR is set independently is not listed in the Application note.

Only <Accelerometer only>, <Gyroscope only> and <Combo [Acc + Gyro]> are shown in Table 6.

I wonder how I can calculate it.

If the Accelerometer's ODR is set to 208Hz and the Gyroscope's ODR is 

set to 

25Hz,

how much power does the sensor consume?

#output-data-rate #lsm6ds3 #power-consumption
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Miroslav BATEK
ST Employee
Posted on September 04, 2017 at 12:33

I'm sorry, I'm not able to provide the current consumption for all combination of  acceleromter and gyroscope ODRs.

But I think you can roughly estimate it from the mentioned table. If you provide me your configuration (Vcc, ODRs, accel. mode) I can also measure it on some sample.