MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LSM9DS1 FIFO

Posted on August 30, 2017 at 18:18I came from using LSM9DS0. I'm a bit confused about how does the FIFO work for gyro and acc in 9DS1. It seems that the FIFO control register only allows me to set 1 watermark/threshold value. Does that mean it appli...

gto by Associate
  • 1244 Views
  • 1 replies
  • 0 kudos

[ATT]9358

Posted on August 29, 2017 at 18:35Dear all,I'm writing .cpp driver for Arduino for the LIS3DHH but something seems wrong.No replies from the accelerometer.Do you have any suggestion on the SPI correct communication task reading my files?

0690X000006080OQAQ.png

shock values LSM6DSL sensor

Posted on August 30, 2017 at 10:17Hi, I would like to know what shock, acceleration and vibration values the LSM6DSL sensor supports. Has anyone used the core IKS01A2 that carries this sensor, with the F401RE? Thank you.#lsm6dsl

Resolved! LSM6DSL inactivity interrupt triggered by activity

Posted on August 26, 2017 at 01:46I'm trying to configure an LSM6DSL device to provide the wrist tilt interrupt on INT2 and the inactivity interrupt on INT1.  The tilt interrupt appears to work fine.  With inactivity however, I see the interrupt whe...

LIS3DHH availability ?

Posted on August 24, 2017 at 09:21Dear ST staff,I'm looking for the LIS3DHH accelerometer on some distributor but no one seems to have it available?Can I buy them directly from ST?It's for a incoming project that is going to produce 3000 pieces for ...

Resolved! How to activate Sensor Hub mode in LSM6DSL

Posted on August 23, 2017 at 16:50Hi!, I'm trying to do bring-up of a board that has the LSM6DSL and other sensors in its sensor hub. I can read and write to other registers except for CTRL10_C (19h) and MASTER_CONFIG (1Ah) which I can only read and...

LIS2DW12 SA0 Pull-Up

Posted on August 24, 2017 at 11:14I have a design in which I have to put the line from SA0 to GND (this is mandatory since the alternate I2C address is already used on my I2C bus). However, the internal pull-up of SA0 seems like it can not be disabl...