MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ASM330LHB performance?

Hello,ASM330LHB 6-axis sensor, can it reach 0.001g?ASM330LHB 6-axis sensor that can reach 0.001g? how high can it reach?Which 6-axis sensor is more accurate?Can they both output angles? This post has been translated from Chinese to comply with the ST...

1232 by Associate
  • 581 Views
  • 1 replies
  • 0 kudos

MEMs Studio and LIS2DUX12, Load Configuration Issue

I am trying to save and reload a configuration file from MEMs Studio into the LIS2DUX12 accelerometer mounted onto the STEVAL_MKI109V3 motherboard. The basic system works fine. When I save a file (either in .json or .ucf format), it all looks correct...

Anti-alias IIS2DLPC

I am trying to configure the IIS2DLPC for anti-aliasing as indicated by figure 3 section 3.4 of an5201.I am seeing frequency folding in the spectrum. I am playing a 300 and 500 Hz sine wave alternately on a sound table to vibrate the sensor. Each ton...

AquaKnott_0-1727894408202.png AquaKnott_2-1727896501799.png

Resolved! Using LSM9DS1 Sensors on the STM32 WB55RG (SPI)

Hello. I wrote the following code to use the LSM9DS1 sensor with the STM32 WB55RG board. The current issue is that when I set the gyro to 0x18 and the accel to 0x28, as specified in the sensor datasheet, the accelerometer and gyro values are swapped ...

junhee by Associate
  • 1029 Views
  • 1 replies
  • 1 kudos

LIS2DUX12 MLC power consumption

Is there any available information about excess power consumption due to the Machine-Learning Core (MLC) on the LIS2DUX12 accelerometer?The LIS2DUX12 datasheet claims in Section 2.2 "Electrical characteristics" a current draw of up to 10.8uA (indepen...

fibo82 by Associate
  • 655 Views
  • 2 replies
  • 0 kudos

LSM6DSV32X Gyroscope Artifacts

We use the accelerometer and gyroscope channels of an LSM6DSV32X for measuring movement parameters of a mechanical system. During some tests we observed artifacts in the gyroscope channel that we cannot explain.Configuration:The LSM6DSV32X is connect...

zeichnung_ta_pendel_aufbau.png rec1.png rec1_signal2_zoomed_annotated.png rec1_signal3.png
JHenn.1 by Associate II
  • 2142 Views
  • 10 replies
  • 0 kudos

STEVAL-STWINKT1 not connecting to dashboard

Hi, I have a STEVAL-STWINKT1BI have flashed,\en.fp-ind-predmnt1.zip\STM32CubeFunctionPack_PREDMNT1_V2.4.1\Projects\STM32L4R9ZI-STWIN\Demonstrations\Predictive_Maintenance_WIFI\AWS\Binary\STM32L4R9ZI-STWIN_PredictiveMaintenance_WIFI_v2.4.1.binI get th...