MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LPS25HB barometer - is it temperature compensated?

Hi. I have two LPS25HB on PCB board. After I cooling them with room air, they show signifacant drop in pressure readings. Do they have full temperature compensation? Are compensation registers protected from accidental erasure?

1.jpg

Accelerometer distortion during high frequency vibrations

We have the following accelerometer in our setup IIS3DHHC - High-resolution, high-stability 3-axis digital inclinometer for industrial applications - STMicroelectronicsExperimental setup:The board in which the accelerometer is integrated is screwed o...

snjl_0-1730709455220.png
snjl by Associate II
  • 1205 Views
  • 4 replies
  • 1 kudos

ST E-compass is available for marine applications ?

I'd like to know if the ST e-compass can be used for marine applications, exactly for position control in a small boat.I already know that it is not moisture proof, but am not sure whether it is available for marine uses.

ThreeE by Associate
  • 614 Views
  • 1 replies
  • 0 kudos

Resolved! LSM6DSL not triggerring interruption

Hello,I having an issue with the LSM6DSL. It's doesn't trigger interruptions on INT1 or INT2.I'm working with the STM32WB10CC and I'm connected through SPI to the LSM6DSL. The SPI is working I'm able to communicate with the sensor but it's not trigge...

Coco by Associate III
  • 1108 Views
  • 2 replies
  • 0 kudos

lsm6dsv16x OIS gyro data thru SPI2

Hello experts, I'd like to ask about lsm6dsv16x OIS gyro data thru SPI2.I could successfully read OIS gyro data thru UI, but I couldn't do it thru SPI2.I checked Mode 3 self test part in lsm6dsv16x  app note, but still I got failed.Could you give som...

How to directly program LSM6DSOX in STEVAL-MKI197V1

Greetings I am reaching out to inquire about the direct programming of the LSM6DSOX chip. I recently acquired the STEVAL-MKI197V1 adapter board, which I have connected to my PC via the STEVAL-MKI109V3 board. I am interested in calculating features on...

MartinR by Associate
  • 789 Views
  • 2 replies
  • 1 kudos

ISM330DLC reads when it is stationary

Hi everyone,I was reading the data from the OUTX/Y/Z_L_A and OUTX/Y/Z_H_A registers. I noticed that if the actual acceleration is some non-zero value, the data will be fine. However, if the accelerometer is stationary, the horizontal axises (which ar...

Screenshot 2024-10-31 at 15.27.16.png
zhan2378 by Associate
  • 633 Views
  • 1 replies
  • 0 kudos

Resolved! ASM330LHH can not updata regiter

... I'm using ASM330LHH chip, I'm using the SPI communication method, when I initialize the write to these registers, I confirm that it has been written, I go to read the STATUS_REG register, and I find that it has always been 0, and then I go to rea...

c458f9db14cea4493516f41adac62ed.png 9ab966ea38871e179c5eeffa9fdf29d.png
doudou by Associate II
  • 928 Views
  • 2 replies
  • 0 kudos