MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Accelerometer ISM330 - Sampling frequency configuration

Hello, In general, I would like to better understand the relationship between the sampling frequencies of the FIFO and the Accelerometer (ISM330) and how to adjust them correctly for my application, could anyone give an example? In my case I have the...

famadeu by Associate
  • 692 Views
  • 1 replies
  • 1 kudos

LIS2DW12 Activity and Free Fall Detection

Can someone help me how to use one interrupt pin for Activity/Inactivity and another for Free Fall detection? I need to use it in the lowest possible possible mode as my device is coin cell battery powered.Regards,Asish Banerjee

ABane.1 by Associate III
  • 571 Views
  • 2 replies
  • 1 kudos

Single and Double tapping on LSM6DSL accelerometer

Hello,  I am trying to detect Single & Double tapping on LSM6DSL accelerometer. I am configuring the relevant registers as follows: CTRL1_XL=0x60TAP_CFG=0x8ETAP_THS_6D= 0x8INT_DUR2=0x45WUP_THS=0x80MD1_CFG=0x48 Every time I tap the accelerometer, and ...

DZado.2 by Associate II
  • 539 Views
  • 1 replies
  • 0 kudos

Resolved! Changing AIS2IH settings on the fly

Hi,We are intending to use AIS2IH for one of our projects.We would like to change some settings while the device is running and see their effects on the performance/power consumption, in order to decide the best settings for our purpose.I would like ...

keremk by Associate
  • 870 Views
  • 2 replies
  • 0 kudos

Synchronize ISM330IS sampling to external signal

HiI'm trying to use two ISM330IS sensors both connected to the same external microcontroller.I want to synchronize accelerometer and gyroscope sampling (and the ISPU) to the processing cycle (1ms) of my controller.They should optimally both start the...

srv by Associate
  • 1501 Views
  • 3 replies
  • 0 kudos

evaluation board for sensors

Hi,I'm working on a prototype of a device. One of this device features is to collect data from gyroscope, accelerometer and e-compass. It is very important that the device will be ultra-low-power. One goal for the prototype is to verify how much ener...

DPiór.1 by Associate III
  • 730 Views
  • 3 replies
  • 1 kudos

Resolved! eCompass compared to a smart phone compass

Hello,I once compared your eCompass application (STM32F401RE/X-NUCEO-IKS01A3) with the compass on my smart phone.The compass on my smart phone behaves much better than the ECompass; it is not affected by rapid changes in the angle of inclination or b...

RGünt.1 by Associate II
  • 728 Views
  • 2 replies
  • 1 kudos

lsm6ds3tr-c FIFO Read Values Occasionally Incorrect

HIWhen using the FIFO mode on the lsm6ds3tr-c sensor, there appears to be an issue where occasionally the pattern value read from the FIFO buffer is incorrect, leading to potential errors in the subsequent data retrieval process. This issue also resu...

deep_sky by Associate
  • 526 Views
  • 0 replies
  • 0 kudos