2024-12-17 6:01 AM
Hello,
I once compared your eCompass application (STM32F401RE/X-NUCEO-IKS01A3) with the compass on my smart phone.
The compass on my smart phone behaves much better than the ECompass; it is not affected by rapid changes in the angle of inclination or by vibrations.
What is the reason for this? Is it due to the sensors or the software?
Solved! Go to Solution.
2024-12-17 6:46 AM
It looks like a 6-axis sensor with a separate magneto sensor. There are 9-axis sensors that feature build-in sensor fusion that might be better.
My smartphone compass sucks. I frequently have to calibrate it and sometimes it points in the wrong direction.
What is your application? Assumptions about the conditions of the device can be used to improve the algorithm. If your application features slow movements you can filter out fast movements, for instance. If your application remains flat you can filter out tilts in certain directions.
2024-12-17 6:46 AM
It looks like a 6-axis sensor with a separate magneto sensor. There are 9-axis sensors that feature build-in sensor fusion that might be better.
My smartphone compass sucks. I frequently have to calibrate it and sometimes it points in the wrong direction.
What is your application? Assumptions about the conditions of the device can be used to improve the algorithm. If your application features slow movements you can filter out fast movements, for instance. If your application remains flat you can filter out tilts in certain directions.
2024-12-30 3:44 AM
In my case, it's an electrically powered vehicle that simply has to drive straight ahead in a given direction off-road.
For example, I can't get app_mems.c (eCompass) to debug.
The debugger does not stop when I set a breakpoint on subsequent function calls because, for whatever reason, the “SensorReadRequest” always has the value 0.:
RTC_Handler(&msg_dat);
Accelero_Sensor_Handler(&msg_dat);
Gyro_Sensor_Handler(&msg_dat);
Magneto_Sensor_Handler(&msg_dat);
Humidity_Sensor_Handler(&msg_dat);
Temperature_Sensor_Handler(&msg_dat);
Pressure_Sensor_Handler(&msg_dat);
I also need direct access to the variable “heading”.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.