2024-12-18 8:49 AM
I am trying to get the an values ready interrupt working, but I cannot seem to find the right configuration of registers. Normal threshold interrupts are working as expected.
After the normal setup and using all different speeds ODR, when setting INT1_CTRL to INT_DRDY_XL active, I do not get any interrupts. The oscilloscope shows no change as well on either H_LACTIVE as well. Is there a sample that can be provided which has a working implementation of the interrupt working? So far all public sources have non working code.
As an MCU I am using an ESP32 and Arduino.
Here is my current initialisation:
Solved! Go to Solution.
2025-01-02 11:41 PM
Thank you for the answer. The internet did not provide any working example.
Thanks for the quick answer!
2024-12-19 9:41 AM
Welcome @schartnerc, to the community!
Unfortunately, the LSM9DS1 was discontinued some time ago, so that no more information is officially available. If you can't find anything in the depths of the never-forgetting internet, probably nobody will be able to help you.
I am extremely sorry not to be able to help you.
Regards /Peter
2025-01-02 11:41 PM
Thank you for the answer. The internet did not provide any working example.
Thanks for the quick answer!