MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS2DW12TR IC capacitance

1) What capacitance does the LIS2DW12TR introduce to the I2C bus lines?2) What is it's maximum bus capacitance threshold in normal I2C mode (100khz)?The datasheet doesn't have info on either of these points. It only quotes that the max bus capacitanc...

Sensitivity of LIS2DW12 Accelerometer

GreetingsI am working with the LIS2DW12 accelerometer. I am using the device in Low Power Mode 1, with a FS = +-4g.According the application note AN5038, page 15, it says that the Low power mode 1, entails a 12 bit value. Thus, using the 16-bit value...

ZAIDS-S23 by Associate III
  • 570 Views
  • 1 replies
  • 0 kudos

Is LSM6DSL Zephyr driver compatible with LSM6DSM?

Hello,Our custom HW uses a LSM6DSM sensor.  There is no existing driving for it in Zephyr, however, the LSM6DSL sensor does. I looked at the differences between the 2 devices and it comes down to the LSM6DSM having 2 extra connection modes (Modes 3 &...

jkullds by Associate II
  • 566 Views
  • 1 replies
  • 0 kudos

LIS2MDL 3-axis magnetometer to calculate Yaw

we are using LIS2MDL magnetometer calculate yaw (Angle) data. we have integrated the LIS2MDL 3-axis magnetometer along with the ISM330DHCX. However, the resulting yaw data fluctuates, even when the sensors are stationary (without motion).From our und...

ssk2024 by Associate
  • 615 Views
  • 1 replies
  • 0 kudos

Resolved! STHS34PF80 cover material

Hi,I'm now evaluating STHS34FP80 on our original board.I've tried PMMA and BK7 glass for cover material but It seems not work well.Is there any proper material for STHS34PF80 cover?If you know the specific material name, please let me know.Thanks,

TomoPi by Associate
  • 640 Views
  • 1 replies
  • 0 kudos

ASM330LHB performance?

Hello,ASM330LHB 6-axis sensor, can it reach 0.001g?ASM330LHB 6-axis sensor that can reach 0.001g? how high can it reach?Which 6-axis sensor is more accurate?Can they both output angles? This post has been translated from Chinese to comply with the ST...

1232 by Associate
  • 507 Views
  • 1 replies
  • 0 kudos

MEMs Studio and LIS2DUX12, Load Configuration Issue

I am trying to save and reload a configuration file from MEMs Studio into the LIS2DUX12 accelerometer mounted onto the STEVAL_MKI109V3 motherboard. The basic system works fine. When I save a file (either in .json or .ucf format), it all looks correct...

Anti-alias IIS2DLPC

I am trying to configure the IIS2DLPC for anti-aliasing as indicated by figure 3 section 3.4 of an5201.I am seeing frequency folding in the spectrum. I am playing a 300 and 500 Hz sine wave alternately on a sound table to vibrate the sensor. Each ton...

AquaKnott_0-1727894408202.png AquaKnott_2-1727896501799.png

Resolved! Using LSM9DS1 Sensors on the STM32 WB55RG (SPI)

Hello. I wrote the following code to use the LSM9DS1 sensor with the STM32 WB55RG board. The current issue is that when I set the gyro to 0x18 and the accel to 0x28, as specified in the sensor datasheet, the accelerometer and gyro values are swapped ...

junhee by Associate
  • 909 Views
  • 1 replies
  • 1 kudos