MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM6DSOX: 3 vs 4 wire SPI configuration

Hello, this should be a basic question but I am pretty new in this field. What are the core difference between a 3 and a 4 wir SPIe configuration for LSM6DSOX? Apart from electrical connection, is there any difference in Firmware design, capabilities...

ANist by Associate III
  • 1302 Views
  • 3 replies
  • 0 kudos

LIS2DH power consumption with 1 axis enabled?

We're evaluating the LIS2DH (and -DE) for a very low-power project, and every uA is precious. We only need readings from one axis, so I am curious as to whether disabling the other two axes would result in power savings. I've tried measuring it her...

eggs by Associate
  • 898 Views
  • 1 replies
  • 0 kudos

BlueNRG-232 tile won't enable

I've had intermittent success at flashing the firmware provided with the DK for the BlueNRG tile (STEVAL-BCN002V1) when attached to the host board. I can see the image file loading on to the device memory followed by a successful verify and sometime...

RGupp by Associate II
  • 691 Views
  • 2 replies
  • 0 kudos

How to use SHT21 humidty sensor with i2c2 on STM32F103?

Hello everyone,I want to receive humidty from SHT21 sensor. I received first or a few data and then this communication stop. Why? Can you help me please ?http://www.farnell.com/datasheets/1780639.pdf this is datasheet of SHT21Thank you

I am using A3G4250D gyroscope in one of our project. I want to know how to convert RAW value read from register OUT_TEMP (26h) to actual temperature values?

I know that OUT_TEMP register in two’s complement format with a sensitivity of -1 LSB/°C but not able to convert to exact temperature value.please provide the calculation to convert from RAW values to temperature value.Thanks in Advance...!!!

DS by Associate
  • 724 Views
  • 1 replies
  • 0 kudos

Resolved! Setting a threshold value

Hi ,i need to know how to set a threshold value for state machine interrupt, can u explain with an example. precisely means setting the value in the register for wakeup statemachine

MKS by Associate II
  • 1529 Views
  • 5 replies
  • 0 kudos