MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How can I reduce the influence of sunlight with the ToF VL53L1X

For my application I use the ToF VL53L1X.I need to measure the distance from 10cm to 1m in front on a plate surface.I have done some characterisations on a distance test bench indoor, and I have obtained good results.For my application I have to use ...

BMith by Associate
  • 1228 Views
  • 1 replies
  • 0 kudos

Problems with Getting Started Application b/w X-NUCLEO-GNSS and B-L475e-IOT01A1. No previous connection to the Internet is done by the B-L475e-IoT node.

The guide/documentation provided talks mainly b/w the X-NUCLEO-GNSS sensor and a NUCLEO board while I am attempting to use the L475e-IoT Node. When interacting with the application on Tera Term, the menu from the example is displayed. However, when a...

MChav.13 by Associate II
  • 1004 Views
  • 2 replies
  • 0 kudos

STEVAL-BCN002V1 Sensor Demo Project Code Walk-through

STEVAL-BCN002V1 Sensor Demo Project Code Walk-throughDear all, I am new to STEVAL-BCN002V1.I will like to inquire if there is any workshop presentation materials or materials which can explain to me the code walk-through for the entire STEVAL-BCN002V...

garyng98 by Associate
  • 613 Views
  • 1 replies
  • 0 kudos

LIS3DHH interrupt always high

Hello, I've successfully initialized LIS3DHH on STEVAL_MKI180V1 board and been reading values from it. I've also enabled the interrupts but they always seem high (I've added a LED to the INT1 line). What I'd like to do is some threshold on movement, ...

AChri.15 by Associate
  • 618 Views
  • 1 replies
  • 0 kudos