MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

[MPU9250][AK8963] Read magnetometer data problem

Hey.I have a small problem with the MPU9250 module, and more specifically AK8963 (Magnetometer). Reading the values ​​measured by the accelerometer and gyro did not cause me major problems and everything works properly. The matter was complicated whe...

MNowa.10 by Associate
  • 2452 Views
  • 1 replies
  • 0 kudos

Resolved! LIS3DH - Error in C-Driver-MEMS

The Standard C platform-independent drivers for MEMS motion and environmental sensorshttps://www.st.com/content/st_com/en/products/embedded-software/mems-and-sensors-software/drivers-for-mems/c-driver-mems.htmlThe LIS3DH Temperature Sensor is connect...

MotionFD and SensorTile compatibility

Hello ST Community,I would like to ask if the (1)SensorTile and/or (2)SensorTile.box are compatible with the MotionFD library?According to the MotionFD user manual, the library uses Accelerometer and Pressure Sensor data to detect a fall, which both ...

DIM by Associate II
  • 632 Views
  • 1 replies
  • 0 kudos

LIS3DH don't send ACK at 9th clock pulse

I am using LIS3DH accemelator to acuqire gravity data. The MCU is NXP MKL16. LIS3DH's pin8 CS is set to high level to communicate with I2C protocol, and pin7 SA0 is set to connect to GND. The SCL and SDA pins are pull up with 4.7K resisttors. After ...

0690X000009Yv7cQAC.png

LIS2DH12 INT1 not sending interrupts

I am trying to configure the LIS2DH12 to send free-fall interrupts but I have not been able to successfully see any interrupts. Here are the register values that I set:CTRL1(0x20) = 0x47 (ODR = 50hz, XYZ enabled)INT1_THS(0x32) = 0x40INT1_DUR...

RKrei by Associate
  • 580 Views
  • 0 replies
  • 0 kudos