User Activity

I can't get the data transmitted faster than every 487ms or about 0.5s. And that's with the Motion Sensor Update Rate set to 40Hz. I've set the DM (Distance Mode) to short (=1), the TimingBudget to 20 ms and the InterMeasurement down to 25ms. The rel...
I understand the data format to be little endian and can someone show where the format is explained? As an example please decode C7 38 which occurred around 17:26:58.Thanksralph
When logging with the app on an iPhone i can't see where the log files are stored. Can you advise where these are stored?Thanks
Communications appears fine; I get the following from BlueNRG-1 ST-LINK Utility (version 2.0.0.0):ST-LINK SN : 067......ST-LINK Firmware version: V2J33M25Conncetd via SWD.SWD Frequency = 100 KHz.Connection mode : Connect with Pre-Reset.Debug in Low P...
I'd like to select the update rate for specific sensors and create a csv file on the iPhone. Sorry this appears to be such a basic question but i am very new at embedded systems development but anxious to have even some small progress. Any effective ...