MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to use the FP-SNS-MOTENVWB1 with STM32CubeIDE?

The archive downloaded here contains projects for various IDEs, including the STM32CubeIDE.https://www.st.com/content/st_com/en/products/embedded-software/mcu-mpu-embedded-software/stm32-embedded-software/stm32-ode-function-pack-sw/fp-sns-motenvwb1.h...

Romain1 by Associate III
  • 1879 Views
  • 5 replies
  • 0 kudos

Where to find STEVAL-MKSBOX1V1 button instructions?

Hi,Does anybody know where I can find the instructions are for the buttons on the SensorTile box? I think I messed up the software of the device by pressing the buttons in random sequences and combinations. It worked when I experimented it for the fi...

DLim.16 by Associate II
  • 2976 Views
  • 8 replies
  • 0 kudos

LMS6DSM

Hello together, I´m evaluating the IMU LMS6DSM for some ACC applications. Therefore I have two Interrupt Scenarios: The slope of the G value change exceeds a certain valueHigh g:The value of the G value exceeds a certain valueFor the LMS6DSM i only f...

LIS3DSH SPI returning only 0s

I am working in a project with the LIS3DSH accelerometer. I have been working with it for some months and had no problems. void LIS3DSH_Class::enableAcc(byte _speed, byte _antialiasingFilter){ digitalWrite(CS_LIS3DSH, LOW); SPI1.transfer(CTRL_REG...

0690X000009jvXDQAY.jpg

Resolved! Long Blocking MotionFX_manger_run() Processing Time

Hi, I am currently having an issue where the MotionFX_manager_run Function is taking 4ms to process, blocking and starving other tasks. I am running at 48MHz on the STM32WB55 using the softfp compilation. How can I reduce the processing time of the f...

0690X00000AqWftQAF.jpg
Daniel L by Associate III
  • 1095 Views
  • 1 replies
  • 0 kudos

LIS2DH Interrupt for 6D movement detection

Hi,I am trying to make the interrupt work on the the Y-Axis, X-Axis, or Z-Axis.Here are the outputs I am getting. Threshold set to 960 mg. So when it gets bellow that threshold I am looking for an interrupt on the Z-axis. 0.280: Acceleration [mg]:14....

Tashfique by Associate II
  • 1338 Views
  • 1 replies
  • 0 kudos

Temperature sensors

Hi. Based on the temperature sensor i would also love to know ​what form of medium would be best for communicating the temperature to the microcontrollers, and their reasons. Thanks

NKenn by Associate
  • 907 Views
  • 1 replies
  • 0 kudos

Problems getting started with Sensor Tile

I am having a hard time getting started with the SensorTile and need some help. I am using CubeMx (v5.3.0) for the STM32L476JGYx selection, and observe the following result when I try to debug -Here is the error message:Here is the test setup:Thought...

0690X00000AppBWQAZ.png 0690X00000AppCKQAZ.jpg
Justin1 by Senior
  • 2405 Views
  • 4 replies
  • 0 kudos