MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to remove Gravity factor from Accelerometer readings .

 I am using the industrial IIS2DH accelerometer in my vibration analysis product. I need only pure acceleration values in all directions. So at any state if the device is stable (or in constant speed), it should give (0.0,0.0,0.0) roughly.

Not outputting data

My LIS3DH is not outputting any data, its displaying a value of 127, any idea why

RNata.15 by Associate II
  • 702 Views
  • 0 replies
  • 0 kudos

LIS3DSH no output data

Hi all,I'm trying to work with the LIS3DSH but i'm not getting any output data.I have verified the SPI is working, I can write to and read back numbers from the registers so I know they are getting set correctly. I'm using the initialisation code bel...

Use MEMS microphone to record audio with STM32F1 MCU

Hi,I'm sorry if i'm asking anyhting newbie. I want to use an STM32 MCU to build a voice recorde application. The data is acquired by a mic and stored in SD Car which connects via SPI with MCU. However, I've some doubts about my application.Since I ne...

MAndr.233 by Associate III
  • 2283 Views
  • 1 replies
  • 0 kudos

LIS3DH Interrupt line

Hi,Is it possible to disable the interrupt line? By default it is Default: push-pull output forced to GND but I would like to be able to make it floating to use the ucontroller gpio connected to INT1 for other purposes like UART TX.Thank you

Life of industrial accelerometer sensor

I am using the industrial IIS2DH accelerometer in my vibration analysis product. In general what would be life time of this sensor in industrial environment where it is measuring the vibration of machinery with standard operating condiiton.

YMand.4 by Associate
  • 1110 Views
  • 1 replies
  • 0 kudos

How to change LSM6DSOX SPI MODE?

Hi,The datasheet says the device is capable of SPI MODE 0 and 3, the default mode is 3. How does one change it to SPI MODE 0? Is it a hardware or software change?Thanks.

DLim.16 by Associate II
  • 966 Views
  • 2 replies
  • 0 kudos