MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! IIS2MDC single measurement current consumption

Hi,We notice IIS2MDC have single measurement mode which can be used for one shot operation. The datasheet also mention how to calculate current consumption for such mode.However we can not find if the sensor will go sleep immediately after measuremen...

Dillah by Associate II
  • 1446 Views
  • 1 replies
  • 0 kudos

Resolved! Is the ODR of LSM6DS3 the same as sampling frequency?

Hello, I want to use a accelerometer which is LSM6DS3, and it's spec says that it's maximum ODR is 6600Hz.So I want to know is the ODR the same as sampling frequency?Or is it just out data rate? And is sampling frequency less than ODR? If so, what's...

Ray Sun by Associate
  • 1365 Views
  • 1 replies
  • 0 kudos

LIS2DS12 Direction of the accelerations?

Use 3-axis acceleration LIS2DS12page 10 figure 2 Pin description in datasheetThe z direction is reversed in the output, but I don't know why.ex) Gravity acceleration is displayed as + g.

LIS3DHTR returns 0xffc0 for all channels

I'm having some issues in trying to get valid data out of the LIS3DH. For some reason I am only receiving a constant value of -1 [0xffc0 10 bits left aligned] on all channels and FIFO slots. I can read/write all other registers just fine, it's just t...

MarkL by Associate
  • 2045 Views
  • 3 replies
  • 0 kudos

How can I select the right Accelerometer?

I am designing a sensor to measure vibration from industrial equipment. The main characteristics of the accelerometer are listed below:- Acceleration Range - up to 8g- Type - Digital- Output Type - I²C, SPI- Axis - X / Y / Z- Bandwidth - minimum of 1...

0690X00000AsIOnQAN.png