User Activity

I have three accelerometers and the circuit is designed according to the datasheet. I have collected the data of three kinds of accelerometers with the vibration test-bed. The sampling frequency of the accelerometers is all set to 800 Hz, placed hori...
Hello, I want to use a accelerometer which is LSM6DS3, and it's spec says that it's maximum ODR is 6600Hz.So I want to know is the ODR the same as sampling frequency?Or is it just out data rate? And is sampling frequency less than ODR? If so, what's...