cancel
Showing results for 
Search instead for 
Did you mean: 

Is the ODR of LSM6DS3 the same as sampling frequency?

Ray Sun
Associate

Hello, I want to use a accelerometer which is LSM6DS3, and it's spec says that it's maximum ODR is 6600Hz.

So I want to know is the ODR the same as sampling frequency?

Or is it just out data rate? And is sampling frequency less than ODR?

If so, what's the maximum sampling frequency is this sensor chip?

Thanks!

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Eleon BORLINI
ST Employee

Hi @Ray Sun​ , in general, for ST sensors the internal sampling frequency (the ADC chain sampling, I mean) is higher (a multiple of) than the maximum ODR. If the sampling frequency were less than the ODR, you will get some identical consecutive data. Regards

View solution in original post

1 REPLY 1
Eleon BORLINI
ST Employee

Hi @Ray Sun​ , in general, for ST sensors the internal sampling frequency (the ADC chain sampling, I mean) is higher (a multiple of) than the maximum ODR. If the sampling frequency were less than the ODR, you will get some identical consecutive data. Regards