MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

What is the proper way of implementing and handling status return values from the VL53L1X ultralight driver (STSW-IMG009)?

From Pololu's Arduino adaptation of the "heavy" driver =) (STSW-IMG007) I gather that the functions in vl53l1_platform.c should return 0 if they succeed and 1 if they fail, so that's what I've done in the ultralight driver. However, some of the other...

JamesLo by Associate II
  • 2837 Views
  • 3 replies
  • 0 kudos

Errors compiling the demo project in Keil Microvision

I Unzipped the supplied demo software package and opened the tilebox project in Keil Microvision. After it autoinstalled all the support packages required I attempted to compile the code as per the readme.txt instruction. It failed due to not being a...

I2C communication issue with H3LIS331DL and/or LSM9DS1TR chips.

I’m trying to read 6 memory addresses I series. They represent appropriate X, Y, Z Accelerations levels. At low speed – up to 50kbps all good and working correctly. However if I increase I2C speed – up to 400 kbps, then I see wrong data being sent fr...

0690X00000As41GQAR.png

Need Help, can pay

Hi, I need help in SPI communication between an acclerometr and my board, Is there any how someone can do it for me, I will be willing to pay them or does STM supports any forums for help this way.Thanks

RNata.15 by Associate II
  • 1319 Views
  • 3 replies
  • 0 kudos

Can we improve the accuracy of vl53l0x?

I want to detect the difference between two objects like flat surface and little projected surface so that i need accuracy in mm.Could we improve the accuracy level of vl53l0x?

NS.16 by Associate II
  • 856 Views
  • 0 replies
  • 0 kudos