cancel
Showing results for 
Search instead for 
Did you mean: 

LIS2DS12 Direction of the accelerations?

Jlee.1572
Associate

Use 3-axis acceleration LIS2DS12

page 10 figure 2 Pin description in datasheet

The z direction is reversed in the output, but I don't know why.

ex) Gravity acceleration is displayed as + g.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Eleon BORLINI
ST Employee

Hi @Jlee.1572​ , the reading is correct. The accelerometer sense the 1g gravity acceleration but in the direction of the reaction constraint exercised by the surface on which you have placed the device (so, bottom-up direction). To understand this, please note that in case you left your device fall (free fall condition), the sensed acceleration will reduce to 0g. Regards