MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Burst Reading the LSM6DSM FIFO

I am reading the LSM6DSM FIFO with the accel and gyro enabled. I burst read 12 bytes using the SPI. One output byte to say to read the fifo then 12 input bytes (6 bytes of accel and 6 bytes of gyro). That works great. I tried reading more than 12 byt...

Can't vary duration on LIS3DH fall detection

I have been trying to setup fall detection interrupt on LIS3DH. I can get it to work but only with specific setup. In particular INT1_DURATION values: 0x05 works (but is too short) so my global setup is ok. But with any other duration values, even ju...

VL53L0X problem connecting to Nucleo F401RE

HiI have been working with the Nucleo F401RE + P-NUCLEO-53L0A1 sampling the VL53L0X, and it was working fine. However interfacing the Nucleo F401RE  to another VL53L0X module (https://picclick.de/VL53L0X-Time-of-Flight-Distance-Sensor-Breakout-GY-VL5...

Aharon1 by Associate II
  • 724 Views
  • 0 replies
  • 0 kudos

Using DHT22(AM2302) sensor

Hi,I'm looking for some example how to use the sensor with STM32 and wonder why all of them, which I've found, are based on the loop not on interrupts.The response is 40 bits and it takes up to several milliseconds to read it, so during the time MCU ...

not getting accelerator axis values

Hi.We have a board based on nordik nrf52840 chip with lis3dh accelerator sensor connected.i took the driver code for lis3dh from STM github and wrote the context functions using nordic sdk 15.2 (I2C bus). First of all i must say that the ADDRESS in ...

eyal.gal by Associate II
  • 3018 Views
  • 8 replies
  • 0 kudos

LSM6DSOX SPI ack

Hi,I am using an LSM6DSOX in SPI mode. I prefer SPI over I2C because it has bigger data transfer rates. Is there any way to be sure that my SPI commands were executed with success? Are they returning something? For example, how can I be sure of the i...