User Activity

Hi,Is it possible to restore STM8S001 for programming after set it to HALT mode?I try to use halt mode for STM8S001 and STM8S003.The programmer worked, when I used __wait_for_interrupt();but stopped after replacing this procedure to __halt();After se...
I use SDK_Chat example (S2LP DK1.2.1\..\S2LPLibrary_Examples) as a base for my project.To increase a Communication range I change next parameters:DATARATE                   38400 (default) to 4800POWER_DBM                  12 (default) to 14RSSI T...
If 1-layer PCB is used for LPS22 or LPS25, the pin 3 connection to GND requires some complication of the PCB.Is this pin 3 really connected to some internal circuit and must be connected to GND or it may stay unconnected?At least, when pin 3 is uncon...
When two Steval-FKI433V2 evaluation boards yet maintain connection, the S2LPRadioGetRssidBm() functions for both boards show about -103dBm...-104dBm. I can't get less RSSI level. Has the least possible RSSI the same value as the receiver sensitivity...
Hello.I want to decrease power consumption of Steval-FKI433V2 and to cut ST-Link PCB part, but later.Conditions:The modified program SDK_Chat.c (from S2-LP DK example) is loaded to the Nucleo uC. Uder this program Nucleo+S2-LP send back received data...