MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I would like to know what device and model to use for an wireless application where I will have 1 stm32 as a master micro controller waiting to receive data and transmit data(two-way communication) from 5 slave stm32 microcontrollers.

The Master stm32 controller need to send talk with the particular slave in order to turn a LED . By using switch,i will turn off the led in the slave controller .The slave has to sent state of led to master controller .There will be cases when maybe ...

Rmajj.1 by Associate II
  • 2937 Views
  • 5 replies
  • 1 kudos

Resolved! Raw data from lsm6dsox

Hello,In my test board, data from accelerometer and magnetometer are stable.But gyro data has many spikes even though it is put in desk and not moving.Do you have any idea for what cause this and how to fix it?lsm6dsox and lis3mdl are used for test.

0693W000005CYLqQAO.png
JPARK.2 by Associate II
  • 2271 Views
  • 3 replies
  • 0 kudos

IIS2DLPCTR: Why are Out_X,Y,Z values are constantly changing?

I got my PCB from the fab today. I am running a test program based on the code in https://github.com/STMicroelectronics/STMems_Standard_C_drivers/blob/master/iis2dlpc_STdC/example/iis2dlpc_read_data_polling.cSince the Sensor-PCB is on my desk with no...

VJaha.1 by Associate II
  • 1699 Views
  • 2 replies
  • 0 kudos

Resolved! How to configure and synchronize LSM6DSO to Raspeberry Pi

Hi everyone!I have a LSM6DSO iNEMO inertial module (purchased in 2015) and I have some problems. I hope someone can help me. 1) Configuration of LSM6DSO. I have installed the Unico GUI program on my Windows PC, to configure my inertial module. When I...

GDa R.1 by Associate II
  • 4667 Views
  • 8 replies
  • 0 kudos

Resolved! IIS3DWB incorrect acceleration readings (documentation mistake?)

The accelerometer is horizontal, in the Z axis 1g and I have about 500 mg in the X axis. I have 3 pieces of accelerometers and in similar positions I have different readings from the X axis.Temperature reads correctly.I found a certain inaccuracy:in ...

0693W000005Bk2KQAS.png 0693W000005Bk2CQAS.png
PSzym.3 by Associate II
  • 2099 Views
  • 4 replies
  • 0 kudos

Resolved! H3LIS200DL interrupt threshold meaning

Hi, all.I am trying to figure out H3LIS200DL interrupt issue. Even if I have set interrupt threshold to high value, I can't see any pulse on INTx line. Also not sure what the INT1_THS register describes. Datasheet shows only 7 bit value.What I have d...

honestech by Associate II
  • 1594 Views
  • 1 replies
  • 0 kudos

How to unbrick a bricked SensorTile

I tried to flash the FP-SNS-ALLMEMS1 firmware (https://www.st.com/content/st_com/en/products/embedded-software/mcu-mpu-embedded-software/stm32-embedded-software/stm32-ode-function-pack-sw/fp-sns-allmems1.html) to a brand new SensorTile over bluetooth...

JBrad.4 by Associate II
  • 4374 Views
  • 13 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.