MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Use RasPi for evaluation of I2C sensors resp. IoT devices

Electronic designers can leverage worldwide “maker�? trend and use off-the-shelf easy-use platforms like Raspberry Pi for IoT demos or for evaluation purposes - at least as a starting point before you select a suitable component and eva board, tools,...

Kersten by Associate II
  • 924 Views
  • 1 replies
  • 1 kudos

FlightSense part with fastest sample rate

My application is uses a linear array (18 sensors) for object presence detection at a fixed distance (~70mm). A range threshold setting is used. The range measurement is not read, only the interrupt is used indicating the presence of a moving object....

CJani.1 by Associate II
  • 2269 Views
  • 4 replies
  • 0 kudos

Issue with flashing sensor tile with st-link and st-flash.

I'm seeing the below issue with flashing firmware on the sensor tile device. I'm trying to test the ble_sampleapp for the sensor tile device. When I use the STM32Cube IDE with a nucleo board as a debugger, I'm able to run the code on the sensor tile ...

PTeja.1 by Associate
  • 1258 Views
  • 1 replies
  • 0 kudos

How to read raw data from LSM6DSL?

LSM6DSL is connected to processor via i2c bus Following are the configuration made in dts and config file:imu: st-lsm6dsl@6b {        compatible = "st,lsm6dsl";        reg = <0x6b>;    };config fileCONFIG_IIO_ST_LSM6DSX=yCONFIG_IIO_ST_LSM6DSX_I2C=yI ...

RMath.3 by Associate
  • 1968 Views
  • 3 replies
  • 0 kudos

Resolved! Coding sensor fusion application on Sensortile.box

In order to do bench-marking of the work of sensor fusion I wanted to create a code application to test it out. The one provided as a part of the phone app doesnt work reliably, also wanted to code it myself. I was checking intro provided on the webs...

VRakc.1 by Associate II
  • 2533 Views
  • 4 replies
  • 0 kudos

How do I initial CS43L22 on STM32F407G?

Hi,I tried couple to run my code, but I can't just hear any noise or beep. I am very new to this.One issue that I found is SPI3->DR is not receiving anything during debugging.Here is my code and correct me,#include <mbed.h>#include<I2C.h>#include <st...

BC.1 by Associate
  • 1605 Views
  • 1 replies
  • 0 kudos

H3LIS200DL doesn't generate an interrupt

I am trying to get an interrupt when exceeds the limit (for test, 1g), but couldn't see any changes on INT1 line.I have configured H3LIS200DL INT1 (INT1_THS is 0x01, INT1_DURATION is 0x03, INT1_CFG is 0x63). I am getting OUT_X, OUT_Y, OUT_Z between -...

honestech by Associate II
  • 1190 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.