MotionMC and MotionEC librabries initialization fail
- August 17, 2020
- 5 replies
- 2499 views
Good afternoon everyone,
I currently trying to implement an application with the ECompass feature using MotionEC library (and MotionMC library to improve precision and reliability of the data).
My initialization failed (it looks like an infinit loop) inside the MotionMC_Initialize or MotionEC_Initialize functions.
I don't understand why, especially because it worked well last week.
The only thing that change between the two version is the CubeMx project, I checked and there is no difference (same pin, same name, same peripherals and same configuration).
I firstly thought that the CRC module were not well initialized, but it is not the case, everything goes well during HAL drivers and peripherals initialization.
Can someone help me understanding what is happening here ?
Thanks,
Have a nice day,
Best regards,
Julien Mongin.