MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

IIS328DQ Threshold Settings

For IIS328DQ, if the threshold is set to 0.25g, does this mean that it will interrupt if either X, Y, or Z changes more than 0.25g? Our application is to detect a vehicle is moving or not. What is the best threshold to set for this application?

KTeng.1 by Associate II
  • 4133 Views
  • 8 replies
  • 0 kudos

Is there any SAI PDM example for STM32MP1?

I'm looking for device tree configuration to acquire 4/6 PDM microphones resulting in an ALSA tdm stream. It's mentioned in the official documentation here(https://www.st.com/content/ccc/resource/training/technical/product_training/group0/30/7d/ca/21...

ARicc.1 by Associate II
  • 3767 Views
  • 6 replies
  • 0 kudos

Lsm6ds3: I'm working on Fifo functionality of Lsm6ds3 for z-axis but when i retrieve values I'm getting higher g values of 2g at steady state. Can somebody explain why such higher values are generated.

I'm using FIFO in continuous mode and when i read from LSM6DS3_ACC_GYRO_FIFO_DATA_OUT_H register most of the times I'm getting constant value of 0x0F from this register at steady state. The values generated at steady state are 2g always.

RK.6 by Associate
  • 1240 Views
  • 1 replies
  • 0 kudos

About accelerometer LIS3DH

I am considering an accelerometer.The accelerometer is experimenting with LIS3DH.I want to mount an acceleration sensor on a surgical light and detect the movement of the lighting part of the surgical light.I want to issue an INT interrupt when the l...

OHide.1 by Associate
  • 1852 Views
  • 1 replies
  • 0 kudos

Hi, I test LPS33HW

What can happens with parameters of this sensor if we place it into a water of swimming pools ( with any concentration of chlorine and other salts) and it stays there months and years ??? Do it need any maintenance or replacement after a period of an...

RPesi.1 by Associate
  • 1197 Views
  • 1 replies
  • 0 kudos