MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS2HH12- Tilt detection with interrupt

Hello everyone, I'm stuck and I need some help. I have the LIS2HH12 accelerometer connected to my raspberry pi via SPI. So far, I have been able to collect real-time accelerometer data . But my goal is to only get data once the accelerometer is title...

Resolved! STEVAL-MKI228KA arduino

Hello,Please , can i use the module STEVAL-MKI228KA (ILPS22QS) with arduino ?Thanks

ljm by Associate III
  • 393 Views
  • 2 replies
  • 0 kudos

Resolved! LSM6DSL gyroscope and rotation order

Hello, I am trying to use the output of the LSM6DSL (accelerometer + gyroscope) to feed an orientation filter. While the accelerometer part is easy to interpret, I am having some trouble with the gyroscope. Apologies if my question is trivial, I have...

AdB by Associate II
  • 1139 Views
  • 7 replies
  • 3 kudos

Resolved! Earbuds

Hi Team,I came across the LSM6DSV16BX, which seems suitable for sports earbuds. Are there any compact earbud-style development boards or hearable devices available on the market?

Resolved! MEMS Acceleromter

Hello,I am looking for MEMS accelerometer for seismic application.We need low noise, up to 100Hz bandwidth, full scale +-2g range.I consider IIS3DHHC as a candidate, which has features as below:3-axis, ±2.5 g full-scaleUltra-low noise performance: 45...

lhagva99 by Associate
  • 740 Views
  • 3 replies
  • 0 kudos

Resolved! lsm6dsv and quaternions and direction of a cube/dice

Hi based on the quaternion/Sensor fusion of LSM6DSV example I developed an application where I display the direction of a cube. Everything works fine, no drift, but: when I take the device move and turn it around, then put it back in the same exact p...

MK..1 by Associate III
  • 575 Views
  • 3 replies
  • 0 kudos

LIS2HH12 Interrupt generation

Hello all,I'm currently using the LIS2HH12 to sense the acceleration on the three axes. My aim is not to continuously read the acceleration value, but is to set a threshold for each axis and receive an interrupt when one of the thresholds is exceeded...

GiorgioR by Associate
  • 834 Views
  • 3 replies
  • 0 kudos

LPS27HHW Pick&Place and conformal coating

I'm trying to use the LPS27HHW in a 1 gram wildlife tracking device (water resistance required) and am wondering (a) how pick&place is supposed to pick up the sensor, and (b) how I can apply automated spray conformal coating to the board. I would hav...

tve by Associate II
  • 1373 Views
  • 5 replies
  • 1 kudos

LIS2DH12TR Dimension Discrepancy

Hello, We received LIS2DH12TR bought from distributor source with full label and full lot code.Our QC team checked with measuring equipment, and we found the height is above the max 1.0mm. Is it considered normal phenomenon?   Referring to photo atta...

LWU.31 by Associate II
  • 579 Views
  • 1 replies
  • 0 kudos