Is there any application note or other information available about the LPS22HB's low current mode, as enabled by LC_EN in RES_CONF register? Other than reducing power consumption, what does it do and specifically, how does it affect performance?
I'm having a problem in a 1 gram tracker that uses an stm32wle5 powered by a 2.4V LTO battery and 4mW solar cell (through bq25504 energy harvesting chip). If the battery discharges below 1.7V ("should never happen"...) the solar cell cannot recharge ...
I'm looking at Appending A.1.10 of AN5457 where the PA matching impedance measurements for the UFQFPN48 package @14dBm and 915Mhz are shown. I cannot match up the points 1 through 5 in figure 80 with the rows 1 through 5 in table 14 below the figure....