MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LSM6DS3 PEDOMETER

Hi,I'm trying to read step counts. I'm executing all pedometer related functions, but I get no any output.Sincerely,TalhaAnd While Loop 

0693W000008x0OXQAY.png 0693W000008x0OhQAI.png 0693W000008x0P6QAI.png
TKCK.1 by Associate III
  • 3621 Views
  • 7 replies
  • 0 kudos

How to use VL53L3 histogram feature?

I understand the VL53L3 can detect multiple objects, and I think it puts ToF information into different buckets. Where can I find more information about this? app notes, register set, driver software, evaluation code? So far I can only see the data s...

charles23 by Associate III
  • 3144 Views
  • 7 replies
  • 2 kudos

VL53L0X 1.8 I2C and XSHUT

We are running the sensor at 3V but the I2C is 1.8V. Does this mean the XSHUT is also 1.8V referenced. Does the XSHUT pull-up go to 3V or 1.8V?ThanksLeon

LWill.2 by Associate II
  • 1614 Views
  • 2 replies
  • 0 kudos

Resolved! LSM6DSM gyroscope random walk, bias stability

The random walk and bias stability of the LSM6DSM gyroscope could notbe found in the data sheet.​Random walk , bias stability of gyroscope Please tell me the reference value.​

totaw.1 by Associate II
  • 7540 Views
  • 11 replies
  • 0 kudos

LSM6DS3 EVB "STEVAL-MKI160V1" communication issue using SPI 4 wire

Hello SThere am using STEVAL-MKI160V1 in which LSM6DS3 is placed and an trying communicate with it over SPI.Physical connections:CS- CSSCL- CLKSDA - SDO of mcSDO - SDI of mcVDD - 3.3VGND - GND SPI Configuration:SPI Freq- 1MHZSlave Select - Active low...

SChin.2 by Associate III
  • 3871 Views
  • 13 replies
  • 0 kudos

Resolved! lis2mdl driver computes the wrong hard iron offsets

lis2mdl_reg.c has an error in the function int32_t lis2mdl_mag_user_offset_set(stmdev_ctx_t *ctx, int16_t *val).The function incorrectly calculates the OFFSET_X_REG_H, OFFSET_Y_REG_H, and the OFFSET_Z_REG_H registers because it converts val[0] to an ...