MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! IIS328DQ Z axis wild numbers

I'm using a IIS328DQ on I2C buss (400KHz). I've got it set up at +-4g 100Hz samplingIt looks like it's doing it's thing correctly BUT for the z axis value. After the interrupt for data, I'm reading the XYZ outputs (MSB first order) and getting00 50...

RLee.4 by Associate III
  • 2983 Views
  • 5 replies
  • 0 kudos

Resolved! How to calibrate the LIS3DHTR accelerometer?

Hi, I'm working with the LIS3DHTR and I'm trying to calibrate the sensor but I couldn't achieve. When I read the output registers I see most of the time a positive acceleration of more or less of 15mg, I know that there is an offset of +-40mg, but in...

AJura.1 by Associate II
  • 2166 Views
  • 2 replies
  • 0 kudos

LIS2DTW12 who-am-i does not return a value

Do you see anything wrong with this 4-wire spi transaction? The LIS2DTW12 is not responding and I do not understand why. It is hooked up to a P-NUCLEO-W55

AAoe.1 by Associate II
  • 1077 Views
  • 1 replies
  • 0 kudos

Resolved! I'm using the LIS3DH. Do I need to provide a 90 mS delay between configuration of CTRL_REG1 and reading the OUT registers or the FIFO to insure stable output ?

I'm using the LIS3DH. The Application Note AN3308 specifies a 90 mS delay time between configuration and reading data in the suggested procedure for performing a self test, (p57 of DocID18198 Rev 3). The delay is, "... for stable output".  Once ODR i...

JMatt by Associate II
  • 1486 Views
  • 2 replies
  • 0 kudos